• Atmel Software Framework

    By:

    Last Published: | Latest Version: 3.42.0.1279

    Provides software drivers and libraries to build applications for Atmel devices. The minimum supported ASF version is 3.35.1.

    Supported Products: Atmel Studio 7.0

  • LUFA Library

    By:

    Last Published: | Latest Version: 17.4.18.170418

    LUFA, the Lightweight USB Framework for AVRs.

    Supported Products: Atmel Studio 7.0

  • Terminal for Atmel Studio

    By:

    Last Published: | Latest Version: 2.8.4

    An extension for a terminal window inside Atmel Studio providing serial port communication.

    Supported Products: Atmel Studio 7.0

  • Microchip Gallery

    By:

    Last Published: | Latest Version: 8.1.0

    Microchip Gallery If you are having trouble installing the extension please go through the following article: https://microchip.secure.force.com/microchipknowledge/articles/en_US/FAQ/Installing-extensions-in-Atmel-Studio-shows-This-extension-is-not-installable-on-any-currently-installed-products

    Supported Products: Atmel Studio 7.0

  • Arduino IDE for Atmel Studio 7

    By:

    Last Published: | Latest Version: 1806.2.1

    An Arduino Compatible Edit, Build and Deployment tool. Works with or without Arduino.ino files. With or without Arduino IDE. Supports all Arduino.cc versions from 1.0 to 1.8.x (+1.9 beta), Atmel Boards, Microchip chipKIT etc. Code optionally remains compatible with the Arduino IDE. Contains many additional features such as intelligent cache,... More information

    Supported Products: Atmel Studio 7.0

  • Git Source Control Provider

    By:

    Last Published: | Latest Version: 1.3.0

    Git Source Control Provider is a plug-in that integrates git with Visual Studio.

    Supported Products: Atmel Studio 7.0

  • Tracealyzer for FreeRTOS

    By:

    Last Published: | Latest Version: 3.2.1

    Get amazing insight into the runtime world of FreeRTOS systems.

    Supported Products: Atmel Studio 7.0

  • Atmel Start

    By:

    Last Published: | Latest Version: 1.0.115

    Atmel START Extension for Atmel Studio

    Supported Products: Atmel Studio 7.0

  • Atmel-USB-Installer-7.0

    By:

    Last Published: | Latest Version: 1.0.0

    Atmel USB Installer

    Supported Products: Atmel Studio 7.0

  • Data Size Viewer

    By:

    Last Published: | Latest Version: 0.12.0

    Displays a list grouped by segment of a compiled application's symbols, and their sizes.

    Supported Products: Atmel Studio 7.0

  • Data Visualizer Extension

    By:

    Last Published: | Latest Version: 2.18.723

    Atmel Data Visualizer is a program used for processing and visualizing data. Data Visualizer can receive data from various sources such as the Embedded Debugger Data Gateway Interface found on XplainedPro boards, and COM ports. Data Visualizer has a graph plotter and an oscilloscope, a terminal and a configurable dashboard with buttons, sliders,... More information

    Supported Products: Atmel Studio 7.0

  • QTouch Library 5.9

    By:

    Last Published: | Latest Version: 5.9.0.211

    Provides libraries for QTouch. The minimum supported ASF version is 3.30.1.

    Supported Products: Atmel Studio 7.0

  • QTouch Composer 5.9

    By:

    Last Published: | Latest Version: 5.9.122

    Provides QTouch Analyzer and QTouch Project Builder. Prerequisites: - Atmel Studio 7.0.1006 or later - Atmel Software Framework v3.30.1 or later - QTouch Library 5.9.0.191 or later

    Supported Products: Atmel Studio 7.0

  • Data Visualizer (Standalone)

    By:

    Last Published: | Latest Version: 2.18.663

    Data Visualizer is a program used for processing and visualizing data. Data Visualizer can receive data from various sources such as the Embedded Debugger Data Gateway Interface found on XplainedPro boards, and COM ports. Data Visualizer has a graph plotter and an oscilloscope, a terminal and a configurable dashboard with buttons, sliders, and... More information

    Supported Products: Atmel Studio 7.0, Atmel Studio 6.2, Atmel Studio 6.1, Atmel Studio 6.0

  • CodeVisionAVR V3.32 Evaluation

    By:

    Last Published: | Latest Version: 3.32.0

    C Compiler and CodeWizard extension for the Microchip/Atmel Studio 7. Supports the Microchip/Atmel Tiny, Mega and Xmega AVR 8-bit Microcontrollers.

    Supported Products: Atmel Studio 7.0, Atmel Studio 6.2

  • Add New File

    By:

    Last Published: | Latest Version: 3.3.0

    The fastest and easiest way to add new files to any project - including files that start with a dot

    Supported Products: Atmel Studio 7.0

  • Naggy

    By:

    Last Published: | Latest Version: 0.4.0

    Compiler diagnostics and preprocessor lowlighting in Atmel Studio for C and C++ projects.

    Supported Products: Atmel Studio 7.0

  • AStyle Extension

    By:

    Last Published: | Latest Version: 2.7.0

    An extension for Artistic Style.

    Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1 , Atmel Studio 6.2 , Atmel Studio 7.0

  • Wireless Composer 7.0

    By:

    Last Published: | Latest Version: 7.0.130

    Provides the Wireless Performance Analyzer and IEEE 802.15.4 MAC Project Wizard. Wireless Performance Analyzer is used to demonstrate various features and capabilities of Atmel IEEE 802.15.4 Transceivers and BLE Transceivers. IEEE 802.15.4 MAC Project Wizard provides user interface to create firmware projects based on AVR2025 MAC stack using Atmel... More information

    Supported Products: Atmel Studio 7.0

  • Build Taskbar Overlay

    By:

    Last Published: | Latest Version: 0.82.0

    Build status overlay on the Windows 7 Taskbar, visually showing when builds are in progress, completed successfully or failed.

    Supported Products: Atmel Studio 7.0