• Wireless Composer

    By:

    Last Published: | Latest Version: 6.1.823

    Provides the Wireless Performance Analyzer and IEEE 802.15.4 MAC Project Wizard. Wireless Performance Analyzer is used to demonstrate various features and capabilities of Atmel IEEE 802.15.4 Transceivers. IEEE 802.15.4 MAC Project Wizard provides user interface to create firmware projects based on AVR2025 MAC stack using Atmel microcontrollers and... More information

    Supported Products: Atmel Studio 6.1

  • Wireshark Sniffer Interface Tool v3.0.0.10

    By:

    Last Published: | Latest Version: 3.0.0.10

    Wireshark Sniffer Interface Tool v3.0.0.10 Wireshark Sniffer Interface Tool has been deprecated. Please use Microchip PCAP Utility(https://gallery.microchip.com/packages/microchippcap-utility/)

    Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1 , Atmel Studio 6.2

  • Create Project From Makefile

    By:

    Last Published: | Latest Version: 1.2.9

    Create project from makefile and select the make file in studio to build the project.

    Supported Products: Atmel Studio 6.2

  • Doxygen Integrator

    By:

    Last Published: | Latest Version: 6.1.0.6

    Generate Doxygen style documentation for a project right from Atmel Studio...

    Supported Products: Atmel Studio 6.1

  • SAM4L-EK - Using the Segment LCD LowPower Features

    By:

    Last Published: | Latest Version: 4.0.0

    The goal of this Hands-on is to: 1) Describe the main features of the Segment LCD Controller (LCDCA). 2) Understand how to configure and use them to maximize power efficiency.

    Supported Products: Atmel Studio 6.2

  • DRT ARM Toolchain

    By:

    Last Published: | Latest Version: 2.1.1705.34

    Build smaller, faster, more energy efficient software for your Atmel SMART MCU without changing your development environment or source code. SOMNIUM have teamed up with Atmel to bring you all the power of SOMNIUM DRT as an Atmel Studio extension. The DRT toolchain extension is the only Atmel Studio/Atmel Software Framework compatible product... More information

    Supported Products: Atmel Studio 7.0

  • FreeRTOS Viewer

    By:

    Last Published: | Latest Version: 1.1.215

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    Supported Products: Atmel Studio 6.1

  • MultiEditing

    By:

    Last Published: | Latest Version: 1.3.0

    Simultaneously edit in more than one location in the editor If you've ever ran into a case where you wanted to quickly change variable names or multiple loop conditions - you can use Multi-Edit to set virtual carets that all behave the same.

    Supported Products: Atmel Studio 7.0

  • AtmelKits

    By:

    Last Published: | Latest Version: 6.2.371

    AtmelKits

    Supported Products: Atmel Studio 6.2

  • SAM D20 Xplained Pro - Smart Sensor

    By:

    Last Published: | Latest Version: 1.1.1

    In this training session we will build a smart sensor application that acquires environmental data: light and temperature. NOTE: More training material available at http://goo.gl/fbgQsE

    Supported Products: Atmel Studio 6.2

  • Editor Enhancements

    By:

    Last Published: | Latest Version: 1.0.18

    Provides additional features such as HTML and URL encodings, transformations and sorting of selected text the editor.

    Supported Products: Atmel Studio 7.0

  • MemoryLogger

    By:

    Last Published: | Latest Version: 1.5.0

    Writes chip memory to file, with selectable viewer applications.

    Supported Products: Atmel Studio 6.0

  • BNO055 Xplained Pro - Data Stream

    By:

    Last Published: | Latest Version: 1.1.0

    This project runs on the SAM D21 Xplained Pro board with a BNO055 Xplained Pro connected to EXT1. Sensor data is streamed on a virtual COM port by the means of USB CDC.

    Supported Products: Atmel Studio 6.2 , Atmel Studio 7.0

  • Save All the Tabs

    By:

    Last Published: | Latest Version: 1.1.0

    Quickly save and restore sets of document tabs.

    Supported Products: Atmel Studio 7.0

  • MSYS GNU Utilities

    By:

    Last Published: | Latest Version: 1.0.11

    Configure ShellUtils Packages from Tools->Options->Builder->GNU Make and select MSYS_GNU_Utilities. MSYS is a collection of GNU utilities such as bash, make, gawk and grep to allow building of applications and programs which depend on traditionally UNIX tools to be present. It is intended to supplement MinGW and the deficiencies of the cmd shell.... More information

    Supported Products: Atmel Studio 7.0 , Atmel Studio 6.2

  • Create Project From Makefile (Beta)

    By:

    Last Published: | Latest Version: 1.1.0

    Create project from makefile and select the make file in studio to build the project.

    Supported Products: Atmel Studio 6.0

  • BMF055 Example Project - Motion Interrupt

    By:

    Last Published: | Latest Version: 1.1.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to setup the motion interrupts for BMF055 sensor.

    Supported Products: Atmel Studio 6.2 , Atmel Studio 7.0

  • FreeRTOS Viewer

    By:

    Last Published: | Latest Version: 1.0.82

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    Supported Products: Atmel Studio 6.0

  • BMF055 Example Project - Data Stream

    By:

    Last Published: | Latest Version: 1.1.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to configure BMF055 sensor to read raw sensor data and print the results in a terminal software running on a host computer.

    Supported Products: Atmel Studio 6.2 , Atmel Studio 7.0

  • Create Project From Makefile

    By:

    Last Published: | Latest Version: 1.2.5

    Create project from makefile and select the make file in studio to build the project.

    Supported Products: Atmel Studio 6.1