Last Published: | Latest Version: 7.0.1
Generate Doxygen style documentation for a project right from Atmel Studio...
Supported Products: Atmel Studio 7.0
Search Index last updated
Last Published: | Latest Version: 7.0.1
Generate Doxygen style documentation for a project right from Atmel Studio...
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 14.9.3
Adds vertical lines at each indent level.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 7.0.130
Provides the Wireless Performance Analyzer and IEEE 802.15.4 MAC Project Wizard. Wireless Performance Analyzer is used to demonstrate various features and capabilities of Atmel IEEE 802.15.4 Transceivers and BLE Transceivers. IEEE 802.15.4 MAC Project Wizard provides user interface to create firmware projects based on AVR2025 MAC stack using Atmel... More information
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.2.49
Create project from makefile and select the make file in studio to build the project.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 2.7.0
An extension for Artistic Style.
Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1 , Atmel Studio 6.2 , Atmel Studio 7.0
Last Published: | Latest Version: 12.0.0.20210426
A tool to format C/C++/Obj-C code.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.1.106
An extension for debugging with annotated assembly files. This will allow for the user to follow the debugger in the source file and an annotated assembly file. When the debugger breaks it will highlight the breakline and breakpoints in the annotated assembly files.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.0.0
This training module introduces Atmel Peripheral Touch Controller (PTC) of new generation AVR devices. This training module consists of: 1. Procedure to create a QTouch Project using QTouch project builder wizard 2.Analysis of touch data on QTouch Analyzer 3. Understanding QTouch Library API and Sensor Individual parameters 4.... More information
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 2.0.1
This hands-on will demonstrate the ease of use of the different Atmel QTouch technology tools which are used to develop and tune capacitive buttons, sliders and wheels designs, providing within Atmel Studio the most advanced integrated environment for developing touch-enabled AVR or Cortex-M processor-based applications.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.8.0
Stops a solution build immediately after a project has failed to build. Forked from https://github.com/einaregilsson/StopOnFirstBuildError to add Atmel Studio as a installation target.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 0.82.0
Build status overlay on the Windows 7 Taskbar, visually showing when builds are in progress, completed successfully or failed.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 2.1.1.195
Work with output data / log files never been so simple!
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 7.0.1
Writes chip memory to file, with selectable viewer applications.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.4.23
Shows how easy you can make the same action using only the keyboard. Displays the keyboard shortcut for any command that you execute to help you learn the shortcuts you need the most.
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 4.7.3.99
Atmel ARM GNU Toolchain 4.7.3.99
Supported Products: Atmel Studio 7.0, Atmel Studio 6.2, Atmel Studio 6.1, Atmel Studio 6.0
Last Published: | Latest Version: 2.1.1705.34
Build smaller, faster, more energy efficient software for your Atmel SMART MCU without changing your development environment or source code. SOMNIUM have teamed up with Atmel to bring you all the power of SOMNIUM DRT as an Atmel Studio extension. The DRT toolchain extension is the only Atmel Studio/Atmel Software Framework compatible product... More information
Supported Products: Atmel Studio 7.0
Last Published: | Latest Version: 1.0.0
Provides a empty GAS (.S) file.
Supported Products: Atmel Studio 6.0, Atmel Studio 6.1, Atmel Studio 6.2, Atmel Studio 7.0
Last Published: | Latest Version: 1.3.0
Simultaneously edit in more than one location in the editor If you've ever ran into a case where you wanted to quickly change variable names or multiple loop conditions - you can use Multi-Edit to set virtual carets that all behave the same.
Supported Products: Atmel Studio 7.0