gravatar

178

Packages

2,060,607

Downloads of Microchip's packages

Microchip's Profile

Packages (Page 5 of 9) Show all packages

  • SAM D20 Xplained Pro - Smart Sensor Latest version: 1.1.1

    In this training session we will build a smart sensor application that acquires environmental data: light and temperature. NOTE: More training material available at http://goo.gl/fbgQsE

    2,654 downloads

  • Editor Enhancements Latest version: 1.0.18

    Provides additional features such as HTML and URL encodings, transformations and sorting of selected text the editor.

    2,631 downloads

  • MemoryLogger Latest version: 1.5.0

    Writes chip memory to file, with selectable viewer applications.

    2,571 downloads

  • BNO055 Xplained Pro - Data Stream Latest version: 1.1.0

    This project runs on the SAM D21 Xplained Pro board with a BNO055 Xplained Pro connected to EXT1. Sensor data is streamed on a virtual COM port by the means of USB CDC.

    2,484 downloads

  • Save All the Tabs Latest version: 1.1.0

    Quickly save and restore sets of document tabs.

    2,446 downloads

  • MSYS GNU Utilities Latest version: 1.0.11

    Configure ShellUtils Packages from Tools->Options->Builder->GNU Make and select MSYS_GNU_Utilities. MSYS is a collection of GNU utilities such as bash, make, gawk and grep to allow building of applications and programs which depend on traditionally UNIX tools to be present. It is intended to supplement MinGW and the deficiencies of the cmd shell. F... More information

    2,432 downloads

  • Create Project From Makefile (Beta) Latest version: 1.1.0

    Create project from makefile and select the make file in studio to build the project.

    2,413 downloads

  • BMF055 Example Project - Motion Interrupt Latest version: 1.1.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to setup the motion interrupts for BMF055 sensor.

    2,313 downloads

  • BMF055 Example Project - Data Stream Latest version: 1.1.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to configure BMF055 sensor to read raw sensor data and print the results in a terminal software running on a host computer.

    2,306 downloads

  • FreeRTOS Viewer Latest version: 1.0.82

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    2,297 downloads

  • Create Project From Makefile Latest version: 1.2.5

    Create project from makefile and select the make file in studio to build the project.

    2,271 downloads

  • HEXClassifier Latest version: 0.2.0

    Provides syntax highlighting for Intel HEX and Motorola SREC files.

    2,262 downloads

  • Atmel Spaces Add-In for Atmel Studio Latest version: 1.2.1

    Atmel Spaces Add-In for Atmel Studio

    2,247 downloads

  • SAM D21 Xplained PRO -USB Host Bootloader Training Latest version: 1.0.1

    This hands-on training will guide to develop a USB Host bootloader project for SAM D21 device. We are going to develop a bootloder that can detect a mass storage device(for example a USB thumb-drive) when connected to the USB-port. If this device contains an updated firmware image, the bootloader can update the flash of the device wi... More information

    2,190 downloads

  • XMEGA-A3BU Xplained - Sensor Acquisition Latest version: 1.1.0

    "Sensor Acquisition in Time Critical Applications" focuses on data acquisition applications where high performance and deterministic response to time events is critical. NOTE: More training material available at http://goo.gl/fbgQsE

    2,099 downloads

  • BMF055 Example Project - BSX Lite Integration Latest version: 1.2.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to integrate BSX-Lite library in the BMF055 smart sensor.

    2,063 downloads

  • Sensirion Xplained Pro RH/T Latest version: 2.0.1

    Driver and sample application for the Sensirion SHTC1 and SHTW1 extension boards for the Xplained Pro development platforms. - SAM D20 Xplained Pro - ATSAMD20J18

    2,053 downloads

  • MCC Standalone (Linux) Latest version: 5.1.6

    The installer for MPLAB Code Configurator’s standalone application, used to easily generate C code for projects with Microchip devices.

    2,043 downloads

  • MemoryLogger Latest version: 1.9.0

    Writes chip memory to file, with selectable viewer applications.

    2,000 downloads

  • HID Report Writer - Beta Latest version: 1.2.47

    Supports send and receive HID raw reports

    1,973 downloads