gravatar

178

Packages

2,059,270

Downloads of Microchip's packages

Microchip's Profile

Packages (Page 6 of 9) Show all packages

  • CppCheck Integrator (Beta) Latest version: 1.0.0.9

    The extension integerates CppCheck with Atmel Studio and provides a quick and easy way to perform a static code analysis.

    1,920 downloads

  • App Launcher Plugin Latest version: 1.2.0

    The App Launcher is a simple plug-in provides the ability to launch any application within MPLAB X IDE. The App Launcher provides default applications but you can configure any number of applications. Launching the App Launcher Plug-in First, install the launcher plug-in under the MPLAB X IDE. (For installation instructions for plug-ins, refer to ... More information

    1,893 downloads

  • Getting Started with the SAM4L-EK Demo Latest version: 2.0.0

    The goal of this hands-on is to: • Become familiar with the Atmel SAM4L-EK Evaluation Kit • Run and test the SAM4L-EK Demo • Compare the measured current consumption values with the datasheet figures

    1,868 downloads

  • SAM D20 Xplained Pro - Introduction to FreeRTOS Latest version: 1.0.1

    The goals of this hands-on training are: 1) Explain how to Create and configure a FreeRTOS Project under AS 6.1. 2) Give an overview of FreeRTOS mechanism. 3) Explain how to use FreeRTOS and its kernel Object. 4) Show how to make use of FreeRTOS+Trace for Real time project debugging.

    1,721 downloads

  • PWM Implementation using SAM D21 TCC Latest version: 1.1.0

    The goal of this hands-on is to: • Create a Touch project using QTouch Project Builder • Use QTouch Analyzer to test the project • Implement a PWM signal using the SAM D21 Timer/Counters for Control peripheral (TCC) to drive the brightness of a LED • Modify the LED brightness in relation to the Touch Delta value of a Button sensor by u... More information

    1,697 downloads

  • Bootloader-PC-Tool-Setup Latest version: 1.2.2.235

    The Bootloader PC tool is a PC application that is used to load a firmware image to a device. Connection to the MCU shall be enumerated as a COM or USB port depending on the interface used. Source firmware images shall be in the Motorola S-record (SREC) format. Such images are created during compilation further to .hex and .elf images. A device mus... More information

    1,628 downloads

  • Graphics Display Designer X Latest version: 1.10.0

    The Graphics Display Designer X (GDD X) is a MPLAB X IDE plug-in that provides you a quick and easy way of creating graphical user interface (GUI) screens for embedded applications on Microchip microcontrollers. The GDD X is a visual design tool created for use with the Microchip Graphics Library.

    1,624 downloads

  • Wireless Composer Latest version: 6.0.78

    Provides Wireless Performance Analyzer

    1,542 downloads

  • Help Search Extension Latest version: 2.1.123

    A collection of extensions to the search interface.

    1,453 downloads

  • MPLAB-Touch Latest version: 2.5.4

    The touch plugin allows user to visualize touch tuning data within MPLAB Data Visualizer. The plugin supports two-way communication through which user can modify the touch configuration without having to rebuild the project - thus reduces development and tuning time. The touch project in Microchip Code Configurator (MCC) Harmony or Melody needs to... More information

    1,214 downloads

  • Using SAM-BA on the SAM4L-EK Latest version: 1.1.0

    The goal of this hands-on is to: • Understand how to deploy SAM-BA boot on the SAM4L • Understand the differences in the SAM-BA boot process with other SAM3/SAM4 devices • Modify an existing application in order to make it co-exist with SAM-BA boot in internal flash

    1,168 downloads

  • ATmega88PA DALI slave stack Latest version: 1.0.1

    This application shows DALI slave LED module function that compliant with standard IEC62386. Stack is in common->services folder, drivers in mega->drivers, and others are application. The slave should be controlled by master.

    1,103 downloads

  • mplab-x-sdk Latest version: 6.35.0

    Welcome to the MPLAB X SDK! This software development kit contains documentation, sample code, and precompiled libraries for developing a Plugin for MPLAB X IDE, or a standalone application of the MDBCore API. Please use developers forum on Microchip Website for any help/suggestions on SDK. Important Note for users of SDK: Please use developers f... More information

    1,086 downloads

  • HID Report Writer - Beta Latest version: 1.0.0

    Supports send and receive HID raw reports

    1,044 downloads

  • SAMD11-XPRO - USB Training Latest version: 1.0.0

    This USB training is based on ATSAMD11D14AM device and Atmel QTouch library. This training aims to demonstrate the USB device controller feature of SAM D11 MCU series along with the Peripheral Touch controller (PTC) module to control the PC system volume.

    1,038 downloads

  • Microchip Graphics Display Designer - MLA Latest version: 2.20.1

    The Microchip Graphics Library is highly modular and can be used with Microchip´s 16-bit and 32-bit microcontrollers. It is free for Microchip customers, easy-to-use and has an open documented interface for driver or controller support. The library supports the following features: Pre-made graphics objects Supports multiple fonts and languages User... More information

    1,008 downloads

  • SAM D21 Xplained Pro - TCC Training Latest version: 1.0.0

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.

    999 downloads

  • X2C-Scope Latest version: 1.2.5

    This code example consists of 3 parts: 1. MPLAB X Scope plug-in The Scope plug-in features a Variable Monitor which continuously reads variable(s) from the target and displays the data as numeric value(s). The plug-in also contains an oscilloscope-like GUI including features like channel- & trigger configuration for up to 2 channels and an offset-... More information

    959 downloads

  • Free RTOS Viewer Latest version: 2.4.0

    MPLAB-X RTOS Viewer plug-in supports the presentation of RTOS-related data in a uniform, RTOS independent manner. Added FreeRTOS v9 support

    942 downloads

  • Red Lizard Software Goanna Installer Latest version: 3.6.3

    Goanna Studio for Atmel 6.0 (Free Evaluation)

    887 downloads