178
Packages
2,059,270
Downloads of Microchip's packages
Microchip's Profile
Packages (Page 7 of 9) Show all packages
-
Crash Reporter Beta Latest version: 1.3.0
Provides the crash report of Atmel Studio to its developers. It will send the report to studio development team directly. Atmel support team will contact user for further communication.
-
SHTW2 On Body Detection Latest version: 1.0.0
Driver and On-Body detection demo application for the SHTW2 Xplained Pro Dual Humidity and Temperature Board for the Xplained Pro development platforms. - SAM D20 Xplained Pro - ATSAMD20J18
-
ZllRemote (beta) Latest version: 7.0.8
This tool is used to control color scene attributes of ZLL Light link setup.
-
Introduction to Basic RTOS Features using SAM4L-EK Latest version: 1.0.0
The goal of this hands-on is to: • Explain how to Create and configure a FreeRTOS™ Project under AS 6.1 • Give an overview of FreeRTOS mechanism • Explain how to use FreeRTOS and its Kernel Object • Show how to make use of FreeRTOS+Trace for Real time project debugging
-
SAM D21 Xplained Pro - DMAC Training Latest version: 1.0.3
Hands-on Training material for SAM D21 DMAC
-
Choreo Latest version: 0.1.0
Write macros for Atmel Studio in Python
-
SAM D21 Xplained Pro - TCC Training Latest version: 1.0.1
This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.
-
SAMD11-XPRO - TCC Latest version: 1.0.0
This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications (TCC) present in the SAM D11 devices.
-
IR Remote Control - Philips RC5 Protocol Encoder & Decoder Latest version: 1.0.1
This demo showcases the PIC16F's ability to concurrently perform RC5 encoding and decoding while taking advantage of Microchip's eXtreme Low Power (XLP) sleep mode during idle time. The provided source code is written 100% in ANSI C and is completely interrupt-driven. Demo: IR RC5 Transmitter & Receiver Device: PIC16LF1509-I/P (PDIP Package) IDE... More information
-
MemoryLogger Latest version: 1.20.0
Writes chip memory to file, with selectable viewer applications.
-
WSN-Monitor-Setup Latest version: 1.0.0
WSNMonitor is a PC-based GUI diagnostic application for WSNDemo that is used to display the network topology and other information about the IEEE 802.15.4 network. WSNMonitor displays the IEEE 802.15.4 network graph in real time and updates it automatically as the nodes join or leave. The nodes are represented by icons with the node data tips. WSND... More information
-
MicrochipPCAP-Utility(Windows) Latest version: 1.1.0
Microchip PCAP Utility Tool connects the Wireshark Graphical User Interface (GUI) and the sniffer firmware running on the ZigBit® USB stick. The sniffer captures the packets based on the channel and channel page selection. Captured data is sent to Wireshark software to show the decoded packets on the GUI. The sniffer captures IEEE® 802.15.4, Zigbee... More information
-
SAM D20 XPRO- QTouch Surface-Surface Tracking Latest version: 1.0.0
The QTouch Surface hands-on training session consists of: 1. Procedure to generate a QTouch Surface project using QTouch project builder wizard. 2. Analysis of surface data using QTouch Analyzer. 3. Low Power configuration. 4. OLED Display integration . NOTE: Hardware platform used for this training module is SAM D20 Xplained... More information
-
SAM4L-EK - LP Touch Detection using SleepWalking Latest version: 3.0.0
The goal of this Hands-On is to develop an application based on the SleepWalking™ feature of the SAM4L Peripheral Event System.
-
LSSClassifier Latest version: 0.1.0
Provides syntax highlighting for GCC LSS listing files.
-
PIC12 I2C Master & Slave PWM Demo Latest version: 1.0.0
This demo uses two PIC12LF1822 devices, one as an I2C Master and the other as an I2C Slave. The two devices are connected directly with each other via their respective SDA and SCL pins (no external pull-up resistors are required). The I2C Master writes values into the Slave's I2C buffer which will change the Slave device's PWM output characteristic... More information
-
ELFViewer Plugin Latest version: 1.0.0
Plugin for MPLAB-X that allows visualization of an output ELF file. It shows how your program will be laid out on the actual device. Very useful when writing things like bootloaders. The ELFViewer plugin provides a graphical display of the layout of sections within an ELF format file.It accepts most legal ELF file formats generated by the Microchi... More information
-
Machine Learning Partners Plugin Latest version: 1.2.0
In the modern world there is an incredible amount of data available from a multitude of sensors deployed in embedded devices around the world. The ML Partners Plugin allows you to connect your data to our machine learning partner platforms where you can develop solutions that can be deployed in your embedded application.
-
SAMD11-XPRO - DMAC Latest version: 1.0.0
This hands-on training material will demonstrate the use of DMAC for the data transfer between peripheral and memory. An analog voltage measured using ADC will be transferred to the data buffer in internal SRAM.
-
SAM D21 Xplained Pro DMAC Training Latest version: 1.0.0
Hands-on Training Documentation and Firmware for DMAC peripheral on SAM D21 device. This will demonstrate the use of DMAC for the data transfer between peripheral and memory.