gravatar

178

Packages

2,061,843

Downloads of Microchip's packages

Microchip's Profile

Packages (Page 8 of 9) Show all packages

  • Perform Static Code Analysis in MPLABX using PCLint Latest version: 4.1.0

    PCLint is a plugin that makes the user interface more seamless between the PCLint application and the MPLAB X IDE. Although the Plugin is free you have to purchase the third party PCLint application separately. PC-lint for C/C++ the longest continuously advertised software tool in human history, was first introduced in 1985. It will thoroughly c... More information

    473 downloads

  • DMCI Latest version: 2.71.0

    The Data Monitor and Control Interface (DMCI) provide dynamic input control of application variables in MPLAB IDE projects. Application-generated data can be viewed graphically using any of 4 dynamically-assignable graph windows. Data logging is an important feature for an embedded application. Embedded application requires precise data viewing ... More information

    466 downloads

  • EPD Xplained Pro Example for SAM D20 Latest version: 1.0.1

    EPD Xplained Pro extension board is an e-Paper display (EPD) driving board to connect with Atmel SAM D20 Xplained Pro evaluation kit for user to quickly integrate low power e-Paper display in current designs and projects.

    453 downloads

  • MPLABX Memory Starter Kit Plugin Latest version: 1.8.0

    Designers of Serial EEPROM applications can enjoy the increased productivity, reduced time to market and rock-solid design that only a well thought out development system can provide. Microchip's MPLAB® Starter Kit for Serial Memory Products includes everything necessary to quickly develop a robust and reliable Serial EEPROM design, and greatly re... More information

    405 downloads

  • EPD Xplained Pro Example for SAM4L Latest version: 1.0.1

    EPD Xplained Pro extension board is an e-Paper display (EPD) driving board to connect with Atmel SAM4L Xplained Pro evaluation kit for user to quickly integrate low power e-Paper display in current designs and projects.

    404 downloads

  • HID Report Writer - Beta Latest version: 1.0.0

    Supports send and receive HID raw reports

    399 downloads

  • SCILAB X2C addon Latest version: 2.1.0

    OPEN SOURCE Rapid Prototyping Graphical Programming for any 16 or 32bit Microchip ( includes all Atmel SMART ARM devices and XMEGA) uC based on SCILAB and X2C Rapid Prototyping environment further information can be found on www.sim2tronic.com. known issues: not all SMART ARM demos are working with the latest Atmel Studio 7 ASF bug... More information

    394 downloads

  • Digital-Compensator-Design-Tool Latest version: 1.0.2

    The Digital Compensator Design Tool (DCDT) helps power supply designers by simplifying the overall process of determining the digital compensator coefficients and analyzing the control system performance. The DCDT incorporates all feedback gains and delays to provide the most accurate model of the control system. Along with analyzing the closed loo... More information

    394 downloads

  • MPLABX KeeLoq Plugin Latest version: 0.1.0

    A plugin to configure KeeLoq encoder devices. The KeeLoq tool allows you to quickly configure KeeLoq devices with proper settings and encryption keys. This tool is both a debugging tool and a production tool. The tool can generate assembly configuration files than can be easily downloaded into KeeLoq encoder devices, using a hardware programmer ... More information

    377 downloads

  • Understanding Peripheral Event System on SAM4L-EK Latest version: 1.0.0

    The goal of this hands-on is to: • Give an overview of SAM4L Peripheral Even System mechanism • Illustrate the principle by a concrete example

    374 downloads

  • Power Monitor Plugin for MPLAB X Latest version: 1.3.0

    The Power Monitor monitors power usage of user programs in MPLAB X IDE projects. This plugin is to be used with the REAL ICE with the Power Monitor module. To install: Unzip the downloaded file to a .nbm file to your hard drive. Select Tools > Plugins from the IDE menu. Select the Downloaded tab in the Plugins window. Click the Add Plugins... but... More information

    363 downloads

  • StudioLogCollector-Beta Latest version: 1.0.0

    It will collect all studio logs. Logs will be compressed and saved in desktop. It can be later send it to atmel support team.

    325 downloads

  • Segger JLink Probe Plugin Latest version: 1.2.9

    SEGGER JLink Probe MPLAB X Tool Plug-in

    312 downloads

  • Blink an LED using CCS Plugin within MPLABX Latest version: 1.0.0

    Blink an LED using CCS Plugin within MPLABX In this video tutorial, we demonstrate how to use the CCS C compiler plugin within MPLAB® X! You will learn how to: 1) Install the CCS Plug-in in MPLAB® X 2) Set up a new project in MPLAB® X 3) Add an existing C source file to the project 4) Compile and debug the project 5) Find output files 6) Progr... More information

    311 downloads

  • MS8607 Xplained Pro Example for SAM D20 Latest version: 1.0.0

    The MS8607 peripheral module provides the necessary hardware to interface the MS8607 digital pressure, relative humidity and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The MS8607 sensor is a self-contained pressure, humidity and temperature sensor tha... More information

    302 downloads

  • SEGGER J-Link Debug Probes for MPLABX IDE Latest version: 1.2.4

    SEGGER J-Link debug probes bring JTAG development to MPLAB X IDE. J-Link Debug Probes Supported The following J-Link probe versions and types have been tested and are supported in MPLAB X IDE: Version 9 and newer: J-Link BASE The following J-Link probe versions and types should work in MPLAB X IDE: Version 9 and newer: J-Link PLUS, J-Lin... More information

    301 downloads

  • dsPICWorks Plugin Latest version: 1.2.0

    The dsPIC Works Plug-in integrates dsPIC Works application and lets the user to design the application Download DSPIC Works: http://www.microchip.com/developmenttools/productdetails.aspx?partno=sw300021

    295 downloads

  • KMA36 Xplained Pro Example for SAM D20 Latest version: 1.0.0

    The KMA36 peripheral module provides the necessary hardware to interface the KMA36, A universal magnetic encoder for precise rotational measurement. To any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The KMA36 sensor feature a system-on chip technology that combines a magnetore... More information

    291 downloads

  • MCC Standalone (macOS) Latest version: 5.1.6

    The installer for MPLAB Code Configurator’s standalone application, used to easily generate C code for projects with Microchip devices.

    291 downloads

  • MPLAB® ML Data Collector Latest version: 2.0.116

    The MPLAB® ML Data Collector plugin allows users to capture and upload data from MPLAB® Data Visualizer to the MPLAB® ML Development Suite for developing embedded machine learning (ML) models optimized for Microchip MCUs. License for the ML Development Suite can be purchased on Microchip Direct. First time users can login with their myMicrochip cr... More information

    285 downloads