• MicrochipPCAP-Utility(Linux)

    By:

    Last Published: | Latest Version: 1.1.0

    Microchip PCAP Utility Tool connects the Wireshark Graphical User Interface (GUI) and the sniffer firmware running on the ZigBit® USB stick. The sniffer captures the packets based on the channel and channel page selection. Captured data is sent to Wireshark software to show the decoded packets on the GUI. The sniffer captures IEEE® 802.15.4,... More information

  • PIC12 Complementary Output Generator (COG)

    By:

    Last Published: | Latest Version: 1.0.0

    Code example showing the usage of the Comparator, COG, and ADC modules in a PIC12F752 device. The main focus is generating 2 complementary outputs and using the Comparator output to insert a phase delay into the rising edge of the source PWM used as the time base for the 2 complementary outputs. PIC12F752 ADC + Comparator + COG Demo This demo... More information

    Supported Products: MPLAB X

  • Mikroe CODEGRIP Probe

    By:

    Last Published: | Latest Version: 1.0.1

    Mikroe CODEGRIP Probe enhances capabilities of Microchip’s integrated development environment, adding functionality for communicating with CODEGRIP, Mikroe's programmer & debuger module. For detailed information about plugin please refer to the user manual https://docs.mikroe.com/codegrip-plugin-mplabx/user-manual/

    Supported Products: MPLAB X

  • Red Lizard Software Goanna Installer

    By:

    Last Published: | Latest Version: 3.6.3

    Goanna Studio for Atmel 6.1 (Free Evaluation)

    Supported Products: Atmel Studio 6.1

  • Remote-USB-Debugging (Not Supported)

    By:

    Last Published: | Latest Version: 1.0.16

    Please use MPLAB ICE4 for remote debugging and programming. The Remote-USB-Debugging plug-in allows remote access to Microchip USB-based development tools from within the MPLAB® X IDE. The MPLAB® Communications Library must be installed on the remote machine with which the MPLAB® X IDE on the host machine will be communicating. See the plug-in... More information

    Supported Products: MPLAB X

  • MPLAB® ML Model Builder

    By:

    Last Published: | Latest Version: 1.1.29

    The MPLAB® ML Model Builder plugin allows users to develop and deploy embedded machine learning (ML) models based on sensor data from their application. The ML Model Builder includes tools for data management, model development, model testing, and model deployment. License for the ML Development Suite can be purchased on Microchip Direct. First... More information

    Supported Products: MPLAB X

  • MicrochipPCAP-Utilityx64(MacOS)

    By:

    Last Published: | Latest Version: 1.0.0

    Microchip PCAP Utility Tool connects the Wireshark Graphical User Interface (GUI) and the sniffer firmware running on the ZigBit® USB stick. The sniffer captures the packets based on the channel and channel page selection. Captured data is sent to Wireshark software to show the decoded packets on the GUI. The sniffer captures IEEE® 802.15.4,... More information

    Supported Products: Atmel Studio 7.0

  • Halt Notifier Plugin (Trial)

    By:

    Last Published: | Latest Version: 1.0.8

    The HaltNotifier provides the ability to customize any action when target gets halted. Notifications can be customized with actions e.g. sending mail, audio alert, running scripts based on the users. It requires MPLAB X IDE 3.30 or above. To install: Unzip the downloaded ZIP file to two .nbm files on your hard drive. Select Tools > Plugins from... More information

    Supported Products: MPLAB X

  • CPP Check Source

    By:

    Last Published: | Latest Version: 2.11.1

    The original name of this program is "C++check" but it was later changed to "cppcheck".

    Supported Products: MPLAB

  • MPLAB-MTCH9010-Plugin

    By:

    Last Published: | Latest Version: 1.0.1

    The MTCH9010 Plugin allows user to visualize data and configure the MTCH9010 parameters within MPLAB Data Visualizer. The plugin supports two-way communication through which user can modify the MTCH9010 configuration through Enhanced Configuration Mode without having to rebuild the project - thus reduces development and tuning time.

    Supported Products: MTCH9010, MPLAB X, MPLAB Data visualizer

  • XC-16 Source

    By:

    Last Published: | Latest Version: 1.1.1

    Download the XC-16 Compiler Source. It includes Binutils 2.14 and GCC 4.5.1 modified to support Microchip's 16-bit architecture. Build instructions and simple build script included; your mileage may vary.

    Supported Products: MPLAB