• Stimuli Support

    By:

    Last Published: | Latest Version: 0.9.0

    This extension provides support of the stimuli file supported by the simulator. It adds a file template and language parser.

    Supported Products: Atmel Studio 6.1

  • Using SAM-BA on the SAM4L-EK

    By:

    Last Published: | Latest Version: 1.1.0

    The goal of this hands-on is to: • Understand how to deploy SAM-BA boot on the SAM4L • Understand the differences in the SAM-BA boot process with other SAM3/SAM4 devices • Modify an existing application in order to make it co-exist with SAM-BA boot in internal flash

    Supported Products: Atmel Studio 6.2

  • MPLAB-Touch

    By:

    Last Published: | Latest Version: 2.5.4

    The touch plugin allows user to visualize touch tuning data within MPLAB Data Visualizer. The plugin supports two-way communication through which user can modify the touch configuration without having to rebuild the project - thus reduces development and tuning time. The touch project in Microchip Code Configurator (MCC) Harmony or Melody needs to... More information

    Supported Products: MPLAB X

  • ATmega88PA DALI slave stack

    By:

    Last Published: | Latest Version: 1.0.1

    This application shows DALI slave LED module function that compliant with standard IEC62386. Stack is in common->services folder, drivers in mega->drivers, and others are application. The slave should be controlled by master.

    Supported Products: Atmel Studio 6.1

  • HID Report Writer - Beta

    By:

    Last Published: | Latest Version: 1.0.0

    Supports send and receive HID raw reports

    Supported Products: Atmel Studio 6.2

  • SAMD11-XPRO - USB Training

    By:

    Last Published: | Latest Version: 1.0.0

    This USB training is based on ATSAMD11D14AM device and Atmel QTouch library. This training aims to demonstrate the USB device controller feature of SAM D11 MCU series along with the Peripheral Touch controller (PTC) module to control the PC system volume.

    Supported Products: Atmel Studio 6.2

  • Microchip Graphics Display Designer - MLA

    By:

    Last Published: | Latest Version: 2.20.1

    The Microchip Graphics Library is highly modular and can be used with Microchip´s 16-bit and 32-bit microcontrollers. It is free for Microchip customers, easy-to-use and has an open documented interface for driver or controller support. The library supports the following features: Pre-made graphics objects Supports multiple fonts and languages User... More information

    Supported Products: MPLAB X

  • SAM D21 Xplained Pro - TCC Training

    By:

    Last Published: | Latest Version: 1.0.0

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.

    Supported Products: Atmel Studio 6.2

  • X2C-Scope

    By:

    Last Published: | Latest Version: 1.2.5

    This code example consists of 3 parts: 1. MPLAB X Scope plug-in The Scope plug-in features a Variable Monitor which continuously reads variable(s) from the target and displays the data as numeric value(s). The plug-in also contains an oscilloscope-like GUI including features like channel- & trigger configuration for up to 2 channels and an offset-... More information

    Supported Products: MPLAB X

  • Free RTOS Viewer

    By:

    Last Published: | Latest Version: 2.4.0

    MPLAB-X RTOS Viewer plug-in supports the presentation of RTOS-related data in a uniform, RTOS independent manner. Added FreeRTOS v9 support

    Supported Products: MPLAB X

  • Red Lizard Software Goanna Installer

    By:

    Last Published: | Latest Version: 3.6.3

    Goanna Studio for Atmel 6.0 (Free Evaluation)

    Supported Products: Atmel Studio 6.0

  • Crash Reporter Beta

    By:

    Last Published: | Latest Version: 1.3.0

    Provides the crash report of Atmel Studio to its developers. It will send the report to studio development team directly. Atmel support team will contact user for further communication.

    Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1 , Atmel Studio 6.2

  • SHTW2 On Body Detection

    By:

    Last Published: | Latest Version: 1.0.0

    Driver and On-Body detection demo application for the SHTW2 Xplained Pro Dual Humidity and Temperature Board for the Xplained Pro development platforms. - SAM D20 Xplained Pro - ATSAMD20J18

    Supported Products: Atmel Studio 7.0

  • ZllRemote (beta)

    By:

    Last Published: | Latest Version: 7.0.8

    This tool is used to control color scene attributes of ZLL Light link setup.

    Supported Products: Atmel Studio 7.0

  • MPLAB® X SDK

    By:

    Last Published: | Latest Version: 6.30.0

    Welcome to the MPLAB X SDK! This software development kit contains documentation, sample code, and precompiled libraries for developing a Plugin for MPLAB X IDE, or a standalone application of the MDBCore API. Please use developers forum on Microchip Website for any help/suggestions on SDK. Important Note for users of SDK: Please use... More information

    Supported Products: MPLAB X

    803 total downloads

    Tags

  • Introduction to Basic RTOS Features using SAM4L-EK

    By:

    Last Published: | Latest Version: 1.0.0

    The goal of this hands-on is to: • Explain how to Create and configure a FreeRTOS™ Project under AS 6.1 • Give an overview of FreeRTOS mechanism • Explain how to use FreeRTOS and its Kernel Object • Show how to make use of FreeRTOS+Trace for Real time project debugging

    Supported Products: Atmel Studio 6.1

  • SAM D21 Xplained Pro - DMAC Training

    By:

    Last Published: | Latest Version: 1.0.3

    Hands-on Training material for SAM D21 DMAC

    Supported Products: Atmel Studio 6.2

  • Knowles IA611-RDI-01 Xplained Pro Extension – Demo Version

    By:

    Last Published: | Latest Version: 2.0.3

    This is a demo version of the IA611-RDI-01 extension. In order to obtain the full version of the extension, please register at https://solutions.knowles.com/. This reference design is based on the Knowles IA611 smart microphone to enable development of audio-enabled IoT applications. The IA611 bundles a DSP along with a digital microphone in the... More information

    Supported Products: Atmel Studio 7.0

  • Choreo

    By:

    Last Published: | Latest Version: 0.1.0

    Write macros for Atmel Studio in Python

    Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1

  • SAM D21 Xplained Pro - TCC Training

    By:

    Last Published: | Latest Version: 1.0.1

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.

    Supported Products: Atmel Studio 6.2