• HID Report Writer - Beta

    By:

    Last Published: | Latest Version: 1.0.0

    Supports send and receive HID raw reports

    Supported Products: Atmel Studio 6.2

  • Help Search Extension

    By:

    Last Published: | Latest Version: 2.1.123

    A collection of extensions to the search interface.

    Supported Products: Atmel Studio 6.1 , Atmel Studio 6.2

  • SAM D21 Xplained Pro - TCC Training

    By:

    Last Published: | Latest Version: 1.0.0

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.

    Supported Products: Atmel Studio 6.2

  • SAM D21 Xplained Pro - DMAC Training

    By:

    Last Published: | Latest Version: 1.0.3

    Hands-on Training material for SAM D21 DMAC

    Supported Products: Atmel Studio 6.2

  • SAM D21 Xplained Pro - TCC Training

    By:

    Last Published: | Latest Version: 1.0.1

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications(TCC) present in the SAM D21 devices.

    Supported Products: Atmel Studio 6.2

  • SAMD11-XPRO - TCC

    By:

    Last Published: | Latest Version: 1.0.0

    This training hands-on focuses on highlighting the features of the peripheral Timer/Counter for Control Applications (TCC) present in the SAM D11 devices.

    Supported Products: Atmel Studio 6.2

  • SAM D20 XPRO- QTouch Surface-Surface Tracking

    By:

    Last Published: | Latest Version: 1.0.0

    The QTouch Surface hands-on training session consists of: 1. Procedure to generate a QTouch Surface project using QTouch project builder wizard. 2. Analysis of surface data using QTouch Analyzer. 3. Low Power configuration. 4. OLED Display integration . NOTE: Hardware platform used for this training module is SAM D20 Xplained... More information

    Supported Products: Atmel Studio 6.2

  • SAMD11-XPRO - DMAC

    By:

    Last Published: | Latest Version: 1.0.0

    This hands-on training material will demonstrate the use of DMAC for the data transfer between peripheral and memory. An analog voltage measured using ADC will be transferred to the data buffer in internal SRAM.

    Supported Products: Atmel Studio 6.2

  • Crash Reporter Beta

    By:

    Last Published: | Latest Version: 1.3.0

    Provides the crash report of Atmel Studio to its developers. It will send the report to studio development team directly. Atmel support team will contact user for further communication.

    Supported Products: Atmel Studio 6.0 , Atmel Studio 6.1 , Atmel Studio 6.2

  • SAM D21 Xplained Pro DMAC Training

    By:

    Last Published: | Latest Version: 1.0.0

    Hands-on Training Documentation and Firmware for DMAC peripheral on SAM D21 device. This will demonstrate the use of DMAC for the data transfer between peripheral and memory.

    Supported Products: Atmel Studio 6.2

  • MemoryLogger

    By:

    Last Published: | Latest Version: 1.20.0

    Writes chip memory to file, with selectable viewer applications.

    Supported Products: Atmel Studio 6.2

  • MPLAB-Touch

    By:

    Last Published: | Latest Version: 2.5.1

    The touch plugin allows user to visualize touch tuning data within MPLAB Data Visualizer. The plugin supports two-way communication through which user can modify the touch configuration without having to rebuild the project - thus reduces development and tuning time. The touch project in Microchip Code Configurator (MCC) Harmony or Melody needs to... More information

    Supported Products: MPLAB X

  • MS8607 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The MS8607 peripheral module provides the necessary hardware to interface the MS8607 digital pressure, relative humidity and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The MS8607 sensor is a self-contained pressure, humidity and temperature sensor... More information

    Supported Products: Atmel Studio 6.2

  • MS5637 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The MS5637 peripheral module provides the necessary hardware to interface the MS5637 digital barometric pressure and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The MS5637 sensor is a self-contained pressure and temperature sensor that is fully... More information

    Supported Products: Atmel Studio 6.2

  • TSYS02D Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The TSYS02D peripheral module provides the necessary hardware to interface the TSYS02D digital temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The TSYS02D sensor is a self-contained temperature sensor that is fully calibrated during manufacture. The sensor... More information

    Supported Products: Atmel Studio 6.2

  • KMA36 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The KMA36 peripheral module provides the necessary hardware to interface the KMA36, A universal magnetic encoder for precise rotational measurement. To any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The KMA36 sensor feature a system-on chip technology that combines a... More information

    Supported Products: Atmel Studio 6.2

  • HTU2xD Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The HTU21D peripheral module provides the necessary hardware to interface the HTU21D digital relative humidity and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The HTU21D sensor is a self-contained humidity and temperature sensor that is fully... More information

    Supported Products: Atmel Studio 6.2

  • TSYS01 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The TSYS01 peripheral module provides the necessary hardware to interface the TSYS01 digital temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The TSYS01 sensor is a self-contained temperature sensor that is fully calibrated during manufacture. The sensor... More information

    Supported Products: Atmel Studio 6.2

  • BMF055 Example Project - Motion Interrupt

    By:

    Last Published: | Latest Version: 1.0.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to setup the motion interrupts for BMF055 sensor.

    Supported Products: Atmel Studio 6.2

  • StudioLogCollector-Beta

    By:

    Last Published: | Latest Version: 1.0.0

    It will collect all studio logs. Logs will be compressed and saved in desktop. It can be later send it to atmel support team.

    Supported Products: Atmel Studio 6.1 , Atmel Studio 6.2