• Digital-Compensator-Design-Tool

    By:

    Last Published: | Latest Version: 1.0.2

    The Digital Compensator Design Tool (DCDT) helps power supply designers by simplifying the overall process of determining the digital compensator coefficients and analyzing the control system performance. The DCDT incorporates all feedback gains and delays to provide the most accurate model of the control system. Along with analyzing the closed... More information

    Supported Products: MPLAB X

  • MPLABX KeeLoq Plugin

    By:

    Last Published: | Latest Version: 0.1.0

    A plugin to configure KeeLoq encoder devices. The KeeLoq tool allows you to quickly configure KeeLoq devices with proper settings and encryption keys. This tool is both a debugging tool and a production tool. The tool can generate assembly configuration files than can be easily downloaded into KeeLoq encoder devices, using a hardware programmer... More information

    Supported Products: MPLAB X

  • Understanding Peripheral Event System on SAM4L-EK

    By:

    Last Published: | Latest Version: 1.0.0

    The goal of this hands-on is to: • Give an overview of SAM4L Peripheral Even System mechanism • Illustrate the principle by a concrete example

    Supported Products: Atmel Studio 6.1

  • Power Monitor Plugin for MPLAB X

    By:

    Last Published: | Latest Version: 1.3.0

    The Power Monitor monitors power usage of user programs in MPLAB X IDE projects. This plugin is to be used with the REAL ICE with the Power Monitor module. To install: Unzip the downloaded file to a .nbm file to your hard drive. Select Tools > Plugins from the IDE menu. Select the Downloaded tab in the Plugins window. Click the Add Plugins...... More information

    Supported Products: MPLAB X

  • StudioLogCollector-Beta

    By:

    Last Published: | Latest Version: 1.0.0

    It will collect all studio logs. Logs will be compressed and saved in desktop. It can be later send it to atmel support team.

    Supported Products: Atmel Studio 6.1 , Atmel Studio 6.2

  • Segger JLink Probe Plugin

    By:

    Last Published: | Latest Version: 1.2.9

    SEGGER JLink Probe MPLAB X Tool Plug-in

    Supported Products: MPLAB X

  • Blink an LED using CCS Plugin within MPLABX

    By:

    Last Published: | Latest Version: 1.0.0

    Blink an LED using CCS Plugin within MPLABX In this video tutorial, we demonstrate how to use the CCS C compiler plugin within MPLAB® X! You will learn how to: 1) Install the CCS Plug-in in MPLAB® X 2) Set up a new project in MPLAB® X 3) Add an existing C source file to the project 4) Compile and debug the project 5) Find output files 6)... More information

    Supported Products: MPLAB X

  • MS8607 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The MS8607 peripheral module provides the necessary hardware to interface the MS8607 digital pressure, relative humidity and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The MS8607 sensor is a self-contained pressure, humidity and temperature sensor... More information

    Supported Products: Atmel Studio 6.2

  • SEGGER J-Link Debug Probes for MPLABX IDE

    By:

    Last Published: | Latest Version: 1.2.4

    SEGGER J-Link debug probes bring JTAG development to MPLAB X IDE. J-Link Debug Probes Supported The following J-Link probe versions and types have been tested and are supported in MPLAB X IDE: Version 9 and newer: J-Link BASE The following J-Link probe versions and types should work in MPLAB X IDE: Version 9 and newer: J-Link PLUS,... More information

    Supported Products: MPLAB X

  • dsPICWorks Plugin

    By:

    Last Published: | Latest Version: 1.2.0

    The dsPIC Works Plug-in integrates dsPIC Works application and lets the user to design the application Download DSPIC Works: http://www.microchip.com/developmenttools/productdetails.aspx?partno=sw300021

    Supported Products: MPLAB X

  • MCC Standalone (macOS)

    By:

    Last Published: | Latest Version: 5.1.6

    The installer for MPLAB Code Configurator’s standalone application, used to easily generate C code for projects with Microchip devices.

    Supported Products: MPLAB X

  • KMA36 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The KMA36 peripheral module provides the necessary hardware to interface the KMA36, A universal magnetic encoder for precise rotational measurement. To any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The KMA36 sensor feature a system-on chip technology that combines a... More information

    Supported Products: Atmel Studio 6.2

  • MS5637 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The MS5637 peripheral module provides the necessary hardware to interface the MS5637 digital barometric pressure and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The MS5637 sensor is a self-contained pressure and temperature sensor that is fully... More information

    Supported Products: Atmel Studio 6.2

  • MPLAB® ML Data Collector

    By:

    Last Published: | Latest Version: 2.0.116

    The MPLAB® ML Data Collector plugin allows users to capture and upload data from MPLAB® Data Visualizer to the MPLAB® ML Development Suite for developing embedded machine learning (ML) models optimized for Microchip MCUs. License for the ML Development Suite can be purchased on Microchip Direct. First time users can login with their myMicrochip... More information

  • HTU2xD Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The HTU21D peripheral module provides the necessary hardware to interface the HTU21D digital relative humidity and temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The HTU21D sensor is a self-contained humidity and temperature sensor that is fully... More information

    Supported Products: Atmel Studio 6.2

  • WiDBG Setup

    By:

    Last Published: | Latest Version: 1.0.0

    WiDBG(Wireless Debugging), a new debug and analysis solution for IEEE 802.15.4 Wireless stack offerings from Microchip. WiDBG is a comprehensive system that provides both configurable level of debug options with visualization capability and provides remote or proximity based deployment flexibility based on the development environment. Example... More information

    Supported Products: Atmel Studio 6.0

  • TSYS02D Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The TSYS02D peripheral module provides the necessary hardware to interface the TSYS02D digital temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The TSYS02D sensor is a self-contained temperature sensor that is fully calibrated during manufacture. The sensor... More information

    Supported Products: Atmel Studio 6.2

  • BMF055 Example Project - Motion Interrupt

    By:

    Last Published: | Latest Version: 1.0.0

    Sample project for BMF055 – a custom programmable 9-axis motion sensor with Cortex M0+ microcontroller. This project demonstrates how to setup the motion interrupts for BMF055 sensor.

    Supported Products: Atmel Studio 6.2

  • TSYS01 Xplained Pro Example for SAM D20

    By:

    Last Published: | Latest Version: 1.0.0

    The TSYS01 peripheral module provides the necessary hardware to interface the TSYS01 digital temperature sensor to any system that utilizes Atmel Xplained Pro compatible expansion ports configurable for I2C communication. The TSYS01 sensor is a self-contained temperature sensor that is fully calibrated during manufacture. The sensor... More information

    Supported Products: Atmel Studio 6.2

  • ECAN Bit Rate Calculator Plugin

    By:

    Last Published: | Latest Version: 1.3.1

    ECAN Bit Rate Calculator is a plugin to calculate parameters of the ECAN module for 16-bit (dsPIC33F, PIC24H, dsPIC33E, PIC24E) and 32-bit (PIC32MX5XX/6XX/7XX, PIC32MZxxxxECxxxx, PIC32MZxxxxEFxxxx) devices. Given the oscillator frequency, the ECAN time segments, and the Desired Baud Rate, this plugin calculates the Fcan frequency, the Time Quantum... More information

    Supported Products: MPLAB X