• App Launcher Plugin

    By:

    Last Published: | Latest Version: 1.2.0

    The App Launcher is a simple plug-in provides the ability to launch any application within MPLAB X IDE. The App Launcher provides default applications but you can configure any number of applications. Launching the App Launcher Plug-in First, install the launcher plug-in under the MPLAB X IDE. (For installation instructions for plug-ins, refer to... More information

    Supported Products: MPLAB X

  • Perform Static Code Analysis in MPLABX using PCLint

    By:

    Last Published: | Latest Version: 4.1.0

    PCLint is a plugin that makes the user interface more seamless between the PCLint application and the MPLAB X IDE. Although the Plugin is free you have to purchase the third party PCLint application separately. PC-lint for C/C++ the longest continuously advertised software tool in human history, was first introduced in 1985. It will thoroughly... More information

    Supported Products: MPLAB X

  • Power Monitor Plugin for MPLAB X

    By:

    Last Published: | Latest Version: 1.3.0

    The Power Monitor monitors power usage of user programs in MPLAB X IDE projects. This plugin is to be used with the REAL ICE with the Power Monitor module. To install: Unzip the downloaded file to a .nbm file to your hard drive. Select Tools > Plugins from the IDE menu. Select the Downloaded tab in the Plugins window. Click the Add Plugins...... More information

    Supported Products: MPLAB X

  • Graphics Display Designer X

    By:

    Last Published: | Latest Version: 1.10.0

    The Graphics Display Designer X (GDD X) is a MPLAB X IDE plug-in that provides you a quick and easy way of creating graphical user interface (GUI) screens for embedded applications on Microchip microcontrollers. The GDD X is a visual design tool created for use with the Microchip Graphics Library.

    Supported Products: MPLAB X

  • MPLABX Memory Starter Kit Plugin

    By:

    Last Published: | Latest Version: 1.8.0

    Designers of Serial EEPROM applications can enjoy the increased productivity, reduced time to market and rock-solid design that only a well thought out development system can provide. Microchip's MPLAB® Starter Kit for Serial Memory Products includes everything necessary to quickly develop a robust and reliable Serial EEPROM design, and greatly... More information

    Supported Products: MPLAB X

  • ATmega328PB Xplained - Introduction to PTC on AVR

    By:

    Last Published: | Latest Version: 1.0.0

    This training module introduces Atmel Peripheral Touch Controller (PTC) of new generation AVR devices. This training module consists of: 1. Procedure to create a QTouch Project using QTouch project builder wizard 2.Analysis of touch data on QTouch Analyzer 3. Understanding QTouch Library API and Sensor Individual parameters 4.... More information

    Supported Products: Atmel Studio 7.0

  • Blink an LED using CCS Plugin within MPLABX

    By:

    Last Published: | Latest Version: 1.0.0

    Blink an LED using CCS Plugin within MPLABX In this video tutorial, we demonstrate how to use the CCS C compiler plugin within MPLAB® X! You will learn how to: 1) Install the CCS Plug-in in MPLAB® X 2) Set up a new project in MPLAB® X 3) Add an existing C source file to the project 4) Compile and debug the project 5) Find output files 6)... More information

    Supported Products: MPLAB X

  • ELFViewer Plugin

    By:

    Last Published: | Latest Version: 1.0.0

    Plugin for MPLAB-X that allows visualization of an output ELF file. It shows how your program will be laid out on the actual device. Very useful when writing things like bootloaders. The ELFViewer plugin provides a graphical display of the layout of sections within an ELF format file.It accepts most legal ELF file formats generated by the... More information

    Supported Products: MPLAB X

  • SEGGER J-Link Debug Probes for MPLABX IDE

    By:

    Last Published: | Latest Version: 1.2.4

    SEGGER J-Link debug probes bring JTAG development to MPLAB X IDE. J-Link Debug Probes Supported The following J-Link probe versions and types have been tested and are supported in MPLAB X IDE: Version 9 and newer: J-Link BASE The following J-Link probe versions and types should work in MPLAB X IDE: Version 9 and newer: J-Link PLUS,... More information

    Supported Products: MPLAB X

  • MetaOutput

    By:

    Last Published: | Latest Version: 2.1.1.195

    Work with output data / log files never been so simple!

    Supported Products: Atmel Studio 7.0

  • Microchip Graphics Display Designer - MLA

    By:

    Last Published: | Latest Version: 2.20.1

    The Microchip Graphics Library is highly modular and can be used with Microchip´s 16-bit and 32-bit microcontrollers. It is free for Microchip customers, easy-to-use and has an open documented interface for driver or controller support. The library supports the following features: Pre-made graphics objects Supports multiple fonts and languages User... More information

    Supported Products: MPLAB X

  • FreeRTOS Viewer

    By:

    Last Published: | Latest Version: 1.1.520

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    Supported Products: Atmel Studio 6.2

  • MPLAB® ML Model Builder

    By:

    Last Published: | Latest Version: 1.1.29

    The MPLAB® ML Model Builder plugin allows users to develop and deploy embedded machine learning (ML) models based on sensor data from their application. The ML Model Builder includes tools for data management, model development, model testing, and model deployment. License for the ML Development Suite can be purchased on Microchip Direct. First... More information

    Supported Products: MPLAB X

  • Digital-Compensator-Design-Tool

    By:

    Last Published: | Latest Version: 1.0.2

    The Digital Compensator Design Tool (DCDT) helps power supply designers by simplifying the overall process of determining the digital compensator coefficients and analyzing the control system performance. The DCDT incorporates all feedback gains and delays to provide the most accurate model of the control system. Along with analyzing the closed... More information

    Supported Products: MPLAB X

  • MPLABX KeeLoq Plugin

    By:

    Last Published: | Latest Version: 0.1.0

    A plugin to configure KeeLoq encoder devices. The KeeLoq tool allows you to quickly configure KeeLoq devices with proper settings and encryption keys. This tool is both a debugging tool and a production tool. The tool can generate assembly configuration files than can be easily downloaded into KeeLoq encoder devices, using a hardware programmer... More information

    Supported Products: MPLAB X

  • MPLAB-MTCH9010-Plugin

    By:

    Last Published: | Latest Version: 1.0.1

    The MTCH9010 Plugin allows user to visualize data and configure the MTCH9010 parameters within MPLAB Data Visualizer. The plugin supports two-way communication through which user can modify the MTCH9010 configuration through Enhanced Configuration Mode without having to rebuild the project - thus reduces development and tuning time.

    Supported Products: MTCH9010, MPLAB X, MPLAB Data visualizer

  • FreeRTOS Viewer

    By:

    Last Published: | Latest Version: 1.1.215

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    Supported Products: Atmel Studio 6.1

  • PIC12 I2C Master & Slave PWM Demo

    By:

    Last Published: | Latest Version: 1.0.0

    This demo uses two PIC12LF1822 devices, one as an I2C Master and the other as an I2C Slave. The two devices are connected directly with each other via their respective SDA and SCL pins (no external pull-up resistors are required). The I2C Master writes values into the Slave's I2C buffer which will change the Slave device's PWM output... More information

    Supported Products: MPLAB X

  • SAM D20 Xplained Pro - Smart Sensor

    By:

    Last Published: | Latest Version: 1.1.1

    In this training session we will build a smart sensor application that acquires environmental data: light and temperature. NOTE: More training material available at http://goo.gl/fbgQsE

    Supported Products: Atmel Studio 6.2

  • FreeRTOS Viewer

    By:

    Last Published: | Latest Version: 1.0.82

    This extension automatically retrieves and interprets kernel data structures when FreeRTOS source code is broken in the source debugger.

    Supported Products: Atmel Studio 6.0